Privacy Note for
SITRANS mobile IQ
Last update: November 28
th
, 2023
Privacy Notice, privacy policy
Protecting the security and privacy of your personal data is important to SIEMENS AG, Werner-von-
Siemens-Strasse 1, 80333 München, Germany (“
Siemens
”). Therefore, Siemens operates the
SITRANS mobile IQ (“
App
”) in compliance with applicable laws on data protection and data security.
Categories of personal data processed, purpose of the processing and legal basis
When downloading, installing, and using the App, Siemens processes the following personal data
about you:
Location Data:
Precise Location, meaning information which describes the location of a user
or device with the same or grater resolution as a latitude and longitude with three or more
decimal places.
We process your personal data as follows for the following three purposes:
First purpose: activation of Bluetooth®
The App requires that Bluetooth® on your device is enabled and that the App can via
Bluetooth® connect to instrument(s) in range, e.g., SITRANS LR1xx, LR5xx, LG250,
SITRANS AW050 Bluetooth® adapter connected to a SITRANS PS100 or PS2,
SITRANS LU240, SITRANS Verificator, etc.
The App uses the Bluetooth® connectivity to change the parameters of the connected
devices, initiate (automated) tests, download technical data from connected
instrument(s) to the app installed on your device (e.g., serial number for identification
of the connected instrument, parameter, settings, echo profiles, etc.) and allows you
to save this data in the internal storage of your device. If you were using the cloning
function of the App – technical data like e.g., settings can be uploaded via Bluetooth®
from the App to instrument(s) connected to your device. In connection with a
SITRANS Verificator, the App also supports the license activation process and
transfers licenses from a WIBU server to the Verificator.
Even when the App is closed, Bluetooth® interface of your device usually will remain
active. With activated Bluetooth®, your device is potentially visible to third parties,
which hereby might determine the location of your device precisely.
Second purpose: support of onboarding devices to SIWA Blockage Predictor
The App supports the onboarding of instruments to the SIEMENS App SIWA
Blockage Predictor (
https://new.siemens.com/global/en/markets/water.html
)
as follows: while being connected to an instrument e.g. for commissioning purposes,
the user of the App can choose to export to the App SIWA blockage predictor:
i.
all available information of that individual instrument, including e.g., serial
number, tag name, settings, etc.
ii.
the geo location as provided from the mobile device.
When initiating the export, the internet browser and connectivity of the mobile device
are being used to call the App SIWA blockage predictor. As prerequisite, the user
must be a registered user of the App SIWA blockage predictor and must enter his
credentials first before the export will take place. The data transmission is encrypted
(https).